最近搜索

    Wood Screws

    Screws have an important role in many industries and have been used for at least 2000 years. It's safe to say that screws are not something new. There are different types of screws, but it is the wood screw that we will refer to most of the time when talking about screws. A screw can be used for many different applications. Some examples are construction, furniture, guitars, and much more.

    Wood Screw

    This is specifically a screw for wood, as the name suggests. There are various wood screw sizes, long wood screws, and small wood screws. The head of the screw is conical or flat. It can be pointed or rounded. The head of the wood screw can also be slotted, which means that there is a slot in the point of the screw that allows the user to drive it into place easier.

    .Wood screws are a type of screw used to join materials together, usually wood. A wide variety of head types and thread profiles are available. They come with either a "coarse" or "fine" thread. The coarse thread is designed to grip wood better than the finer threads. They can be used in softwood applications where they are not as likely to damage the finish of your project (such as trim work). The fine thread is designed for use in hardwoods, where it will not damage the finish on your project when they are screwed into place (such as bookcases).

    Types of Wood Screw Materials

    There are different types of screws for different materials, including:

    Brass wood screws: These are made from brass, a metal alloy consisting of copper and zinc. Brass is inexpensive and resists corrosion well. It is also a softer metal than steel, so it may not be suitable for all applications.

    Stainless steel wood screws: These are made from stainless steel, which is stronger than brass but does not have as good corrosion resistance from water or moisture exposure. Stainless steel wood screws are often used for outdoor projects like decking because they don't rust as easily as brass ones.

    Copper wood screws: Copper has excellent anti-corrosion properties, making it ideal for outdoor applications where there is exposure to water or moisture, such as patios, garden furniture, or decking boards. Copper wood screws also look attractive when used with copper fittings, such as hinges or handles on doors and windows.

    Aluminum Wood Screws: Aluminum is one of the most popular materials in making wood screws due to its durability, corrosion resistance, and low cost. Aluminum is also easy to machine, which makes it easier for manufacturers to produce high-quality products at an affordable price.

    Uses of Timber screws

    Here are the main uses for timber screws:

    • Joinery - Timber screws can join two pieces of wood together by drilling a hole through both pieces of wood and then screwing the head of the timber screw into both pieces of wood. This will hold them together securely.
    • Screwing into Wood - Timber screws can hold any type of wood when you need something secured or secured to something else, like a wall or floor. You simply drill a hole into the piece of wood that you want to secure and then screw it into place using your chosen timber screw.
    篩選條件
    排序方式
    2 / 2
    每頁顯示的結果