網站維護通知 6月22 - 24日
本網站將於6月22日(週六)淩晨03:00 - 6月24日(週一)早上05:00 期間進行系統維護,維護期間您將無法訪問。如因此對您造成不便,我們深表歉意!
本網站將於6月22日(週六)淩晨03:00 - 6月24日(週一)早上05:00 期間進行系統維護,維護期間您將無法訪問。如因此對您造成不便,我們深表歉意!
A power supply in an electronic device which disperses current/voltages among in the equipment or compensates power for the unstable current flow. Its main purpose is to convert the current into the desired amount of voltage. Just like other electronic devices, power supply comes and runs with some accessories. These power supply accessories work with power supply to perform their tasks efficiently. These accessories include plug kits, ac dc adaptor, diode modules, and battery modules etc. One of the major uses of these accessories is to repair the damaged power supply such as mounting kit, cable harness and connector kit.
As mentioned earlier, a power supply runs along with its accessories and components. If we further dive down in the installation and function of power supplier, the accessories are primarily discussed. A power supply comes with automation and control gear, cables and wires to connect it with the circuit, circuit breakers, fuses, thermal management and switches. All these components help the device achieve its task and perform function. The relays and signal conditioning are also managed.
Cctv cameras are applied to provide surveillance to prevent the security threat. The prime function of cctv power supply is to distribute the required rate of current to each camera working in the system. The accessories include wires, cables and circuits to manage current distribution.
The PC power supply is installed in the computer to convert ac current into low power dc voltage to allow the components of the computer to run. The PSU accessories include transformer, filter, rectifier, PSU cable or pc cord and regulating circuits. All these collectively help maintain a sustainable voltage.
Different brands offer power supply kits which include different voltage regulators. Some adapters provide ac to dc and dc to ac. The power supplies are also called ac dc adapters. These adapters are responsible for the conversion of ac dc current. The adapters are basically the external power suppliers to connect with devices in order to fulfil the need of desired voltages. These ac adapters are responsible for supplying different voltages ranges from 12v adapters to 24v adapters as not all devices need the same rate of voltage to run. The switch adapter is needed to charge the official switch accessories. One good thing about the Nintendo switch adapter is that it is free of the need of custom power adapter. It can easily run on an ordinary type C tip to get charged.
Types of power supply devices
These power supply devices are manifold, but some common examples include:
There are a number of products you could find for your use. These are: