最近搜索

    Laser Measures

    Laser measures are a highly efficient way of measuring distances on all terrains. By using a laser to target and record a point of reference, the device then calculates and displays the distance to that point with a high degree of accuracy. Offering a measurement solution that is far faster and easier than a conventional tape measure, laser measures are highly versatile devices that have proven beneficial to many industries.

    At RS, our range of laser distance measure products features precision models from leading brands, such as Bosch, DeWALT, Leica, Fluke, and RS PRO, with imperial and metric measurement capacities available. If you are looking forward to spending your money in purchasing a high measure laser, you may take a look at the options we offer without keeping a second thought in mind. From this article, we will help you to clarify all doubts that you have in mind, while getting answers to questions such as "Do laser levels measure distance".

    Are laser measures tools accurate?

    Yes, laser measures are well-known for their accuracy. This is another great reason on why people prefer to get them, instead of traditional measuring tools. Wherever precision measurements are required, a digital laser measure can save you time and prevent mistakes.

    How does a laser measure tool work?

    Before you buy a laser tape measure, it is better to have a basic understanding on how it works. Laser distance meters send a laser to a particular point and then, using the time taken for this light beam to return to the device, calculates the distance to a high degree of accuracy. The laser pointer is visible to the human eye and therefore allows the user to easily pinpoint the desired area of measurement, ensuring the measurement is as precise as possible.

    What are the advantages of laser measures?

    You can expect to receive numerous benefits when you are using a laser distance measurer instead of using a traditional method to measure distance. Let's take a quick look at some of the most prominent benefits that you can experience by using a laser for measuring.

    You can easily use it

    Unlike traditional tape measures, laser measures can be used one-handed and do not require anyone to assist with longer measurements. They can also be used in low light, especially when they feature backlit LCD or digital displays. For example, a Leica laser measure can help you to stay away from hassle due to the presence of a lightweight device.

    You don't need to move the reference

    Laser measurement devices can typically record several points of references without having to move, allowing you to calculate relative distances between two points. This can also help you to get a more convenient distance measuring experience out of your Bosch laser measure.

    You can easily carry it wherever you go

    Typically, these devices are pocket-sized with easily read display screens making them easy to use, store and transport, and can even be tripod-mounted for accurate measurements over very long distances. Commercially available products such as Bosch laser measure and Leica measuring device are well-known for their portable dimensions.

    Are there any drawbacks in using a laser ruler?

    When you are using a laser tape, you should also check and see whether there are any drawbacks or not. The only real disadvantage is that they require a battery charge or power source to operate and may be more susceptible to harsh environments than manual measurement tapes. However, environmentally-resistant, and water-resistant laser measures are available.

    1 / 1
    每頁顯示的結果