MCBs

MCBs, or miniature circuit breakers, are a type of switch used to automatically turn off electrical circuits during abnormal conditions. MCBs often replace fuses in low voltage electrical circuits as they can be more reliable, much more sensitive and are resettable.


How an MCB Works


When continuous overcurrent flows through an MCB, a bimetallic strip is heated and causes it to bend. This bending of the bimetallic strip releases a mechanical latch opening the contacts and turning off the MCB, thereby stopping the current to flow in the circuit. To restart the flow of current the MCB must be manually turned on. This mechanism protects the MCB from faults arising due to overcurrent or overload and is intended to prevent the accidental overloading of the cable in a no-fault situation. The speed of the MCB tripping will vary with the degree of the overload. This is usually achieved by the use of a thermal device in the MCB. The second characteristic is the magnetic fault protection, which is intended to operate when the fault reaches a predetermined level and to trip the MCB within one-tenth of a second. The level of this magnetic trip gives the MCB its type characteristic.


MCBs are used to perform many functions such as local control switches, isolating switches against faults and overload protection devices for installation or specific equipment or appliances.


MCB Types


MCBs have three common types for circuit protection in residential, commercial and industrial applications. The use is classified by a type, which determines the tripping characteristics of the MCB:


Type B - trips between 3 and 5 times the load current


This type will trip instantly at a rate of three to five times its rated current. These are normally used for resistive or small inductive loads where switching surges are very small. Therefore, these are suitable for residential or light commercial installations.


Type C - trips between 5 and 10 times the full load current


This type will trip instantly at a rate of five to ten times its rated current. These are normally used for high inductive loads where switching surges are high such as small motors and fluorescent lighting. In such cases, type C MCBs are preferred to handle higher value of short circuit currents. Therefore, these are suitable for highly inductive commercial and industrial installations.


Type D - trips between 10 and 20 times the full load current


This type will trip instantly at a rate of ten to twenty-five times its rated current. These are normally used for very high inductive loads where high inrush current is very frequent. These are suitable for specific industrial and commercial applications. The common examples of such applications include x-ray machines, UPS systems, industrial welding equipment, large winding motors, etc.


How to select a suitable MCB for the application?


Focus on 3 main points to choose the right MCB for the electrical circuit


  1. Ampere rating

  2. Short circuit breaking capacity

  3. Application type

...
顯示內容 隱藏內容

篩選條件

正在檢視 2281 - 2300,共 2318 項產品
Results per page
Description Price Number of Poles Current Rating Model Number Range Series Rated AC Voltage Tripping Characteristics Breaking Capacity Mounting Style Rated DC Voltage Length Width Depth Application
全新
RS庫存編號 2552566534
製造零件編號X22217515 (1)
BrandETA
HK$25.00
單位
- - - - - - - - - - - - - -
全新
RS庫存編號 2552566700
製造零件編號Y30785101 (1)
BrandETA
HK$6.45
單位
- - - - - - - - - - - - - -
全新
RS庫存編號 2552566696
製造零件編號X4230-LT1 (1)
BrandETA
HK$226.00
單位
- - - - - - - - - - - - - -
全新
RS庫存編號 2552566578
製造零件編號X22223201 (1)
BrandETA
HK$151.00
單位
- - - - - - - - - - - - - -
全新
RS庫存編號 2552565336
製造零件編號A9A26924 (1)
HK$323.00
單位
- - - - - - - - - - - - - -
全新
RS庫存編號 2552566467
製造零件編號X22223302 (1)
BrandETA
HK$136.00
單位
- - - - - - - - - - - - - -
全新
RS庫存編號 2552561431
製造零件編號S29329 (1)
HK$356.00
單位
- - - - - - - - - - - - - -
全新
RS庫存編號 2552566591
製造零件編號X22217512 (1)
BrandETA
HK$25.00
單位
- - - - - - - - - - - - - -
全新
RS庫存編號 2552566532
製造零件編號X22217510 (1)
BrandETA
HK$25.00
單位
- - - - - - - - - - - - - -
全新
RS庫存編號 2552566817
製造零件編號X22217607 (1)
BrandETA
HK$66.10
單位
- - - - - - - - - - - - - -
全新
RS庫存編號 2552566690
製造零件編號X4230-BU157P18S (1)
BrandETA
HK$1,693.00
單位
- - - - - - - - - - - - - -
全新
RS庫存編號 2552566535
製造零件編號Y30728001 (1)
BrandETA
HK$12.70
單位
- - - - - - - - - - - - - -
全新
RS庫存編號 2552566697
製造零件編號X4230-LT2 (1)
BrandETA
HK$242.00
單位
- - - - - - - - - - - - - -
全新
RS庫存編號 2552566569
製造零件編號X22217509 (1)
BrandETA
HK$25.00
單位
- - - - - - - - - - - - - -
全新
RS庫存編號 2552566644
製造零件編號X22261102 (1)
BrandETA
HK$327.00
單位
- - - - - - - - - - - - - -
全新
RS庫存編號 2552576161
製造零件編號5SJ4218-7HG42 (1)
BrandSiemens
HK$988.00
單位
- - - - - - - - - - - - - -
全新
RS庫存編號 2552566546
製造零件編號X22211901 (1)
BrandETA
HK$66.50
單位
- - - - - - - - - - - - - -
全新
RS庫存編號 2552559370
製造零件編號KCG2YZ (1)
HK$482.00
單位
- - - - - - - - - - - - - -
全新
RS庫存編號 2552566815
製造零件編號X22217513 (1)
BrandETA
HK$25.00
單位
- - - - - - - - - - - - - -
全新
RS庫存編號 2552566533
製造零件編號X22217519 (1)
BrandETA
HK$25.00
單位
- - - - - - - - - - - - - -