最近搜索

    PLCs - Programmable Logic Controllers

    PLC stands for Programmable Logic Controller. It is a digital computer-based control system commonly used in industrial automation to monitor and control machinery or processes. A PLC is designed to withstand harsh industrial environments and is typically used to automate tasks that require precision, reliability, and flexibility. It consists of a programmable microprocessor, input and output modules, and various communication interfaces.

    How do PLCs (Programmable Logic Controllers) work?

    PLCs (Programmable Logic Controllers) work by executing a program or set of instructions to control and automate industrial processes.

    • Input Acquisition
    • Program Execution
    • Program Logic
    • Decision Making
    • Output Control
    • Communication
    • Monitoring and Diagnostics

    What are the benefits of PLCs (Programmable Logic Controllers)?

    • Flexibility: Provide a high degree of flexibility in terms of programming and reprogramming. They allow for easy modification and adaptation of control logic to accommodate changes in the process or system requirements without requiring hardware modifications.
    • Reliability: Designed for reliable operation in harsh industrial environments. They are built to withstand extreme temperatures, vibration, electrical noise, and other challenging conditions. PLCs are known for their robustness and durability.
    • Real-time Operation: Offer real-time control, enabling precise and timely response to inputs and events. This is crucial in applications that require fast and accurate control, such as high-speed manufacturing processes or critical safety systems.
    • Diagnostics and Troubleshooting: PLCs provide built-in diagnostics and monitoring capabilities, allowing operators to detect faults, analyse performance, and troubleshoot issues quickly. This facilitates maintenance and minimizes downtime.
    • Safety Features: Many PLCs offer safety-oriented functionality, including specialized programming languages and certified safety modules. Safety PLCs ensure compliance with industry safety standards and provide features such as safety interlocks, emergency stop functions, and fault detection.
    • Remote Access and Monitoring: PLCs with network connectivity allow for remote access and monitoring, enabling operators to control and monitor processes from a central location or through secure remote connections. This enhances operational efficiency and facilitates remote troubleshooting.

    What applications use PLCs (Programmable Logic Controllers)?

    • Manufacturing
    • Power Generation and Distribution
    • Chemical and Petrochemical Industry
    • Water and Wastewater Treatment
    • Food and Beverage Industry
    • Automotive Industry
    • Pharmaceutical Industry
    • Packaging and Material Handling
    • Oil and Gas Industry

    More information can be found in our PLCs guide.

    1166 產品顯示為 PLCs - Programmable Logic Controllers

    Better World
    HK$117,407.43
    Schneider Electric
    -
    Modicon M580
    -
    -
    Modicon M580
    -
    Analogue
    -
    -
    24 V dc
    Ethernet
    -
    -
    Yes
    Green Premium
    -
    HK$7,403.36
    Eaton
    -
    EC4P
    12
    Digital
    Machines
    24 V
    Analog/Digital
    -
    -
    -
    -
    -
    -
    -
    -
    -
    HK$1,235.97
    Phoenix Contact
    -
    NLC-IO-06I-04QTP-01A
    4
    Analogue
    Nanoline Base Unit
    24 V
    Analog
    -
    -
    -
    -
    -
    -
    -
    -
    -
    • RS庫存編號 438-888
    • 製造零件編號 BMEECN0100H
    HK$19,199.34
    Schneider Electric
    -
    Modicon M580
    -
    -
    Racks
    -
    -
    -
    -
    -
    -
    -
    -
    -
    -
    -
    • RS庫存編號 609-619
    • 製造零件編號 750-8211
    HK$807,486.47
    WAGO
    -
    -
    -
    -
    -
    -
    -
    -
    -
    -
    -
    -
    -
    -
    -
    -
    HK$10,746.80
    Schneider Electric
    -
    Modicon ABE7
    -
    Current
    Modicon X80
    -
    -
    -
    -
    -
    -
    -
    -
    -
    -
    -
    每頁顯示的結果